State Generation Modules - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The State Generation group of modules determines the current mode of the unit.

The module sections include general information, such as description, attributes, and use in applications. Some modules include an additional reliability section with specific information for that module. Unless otherwise stated, for all other modules, the reliability attribute is generally described as follows.

If the source point of a connection is unreliable, the destination point uses the last reliable value or, if none exists, it uses the Default Value. This process dynamically breaks the connection if the source is not reliable and then remakes the connection when the source becomes reliable. The reliability of all modules reflects the reliability of its outputs. If any output is not reliable, then the module is not reliable. All outputs of the module are associated with the reliability of the module itself and retain their previous values when the outputs are not reliable.

See the Upgrading System Files section for a list and description of the module and System Selection changes that were made since the last release of the tool.