Viewing and Modifying Details - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

You can view and modify details in the Configuration mode, Simulation mode, and Commissioning mode. See Viewing and Modifying Parameters in the Configuring a System section for more information.

Note: System simulation is paused when you transition into Edit mode or open a Command dialog box. Simulation immediately resumes when you exit the window.