Viewing Connections - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
You can view connections in the Configuration mode, Simulation mode, and Commissioning mode. In Simulation mode, the values are shown in real time rather than defaults. See Viewing and Modifying Connections in the Configuring a System section for more information.