Stopping Simulation - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Procedure

  1. Click Configure. The Simulation Exit - Confirmation dialog box appears.
  2. Click Yes to confirm that you want to stop simulation.
  3. If you made changes during the Simulation session, a second Confirm dialog box appears.
  4. Click Yes if you want to apply the changes you made during the simulation session or No to discard the changes.
    Note: At any time, you can close the tool from any mode. If you close from Simulation mode, the tool guides you through these prompts before closing.