See the Commanding Items and Commanding Network Inputs and Network Outputs sections.
|
Field |
Description |
|---|---|
|
Attribute Command |
Use to enter a value to send a test or restore the value. |
| Attribute | Use to choose the attribute to command from the drop-down list box. |
| Details | Shows the value entered for the test command. |
| Test | Use to test a value for the command. |
| Value | Use to enter the value for the test. |
| Restore | Restores the value to the default. |
|
OK |
Opens a second screen with more command choices based on your selections. |
|
Cancel |
Closes the screen without applying the changes. |
|
|
Opens the Help system. |