Adjust Refresh Rate Dialog Box - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
See the Adjusting the Simulation and Commissioning Refresh Rates section.

Table 1. Adjust Refresh Rate Dialog Box

Field

Description

Simulation Refresh Rate Slider Bar

Use to adjust the simulation refresh rate to any length of time from 1 to 60 seconds.

Commissioning Refresh Rate Slider Bar

Use to adjust the commissioning refresh rate to any length of time from 1 to 60 seconds.

Highlight Duration Slider Bar

Use to adjust the highlight duration rate for changing parameter values displayed in the Simulation and Commissioning modes. Highlight duration refresh rates range from 1 logic cycle to 10 logic cycles in length.

Note: The highlighting change feature can be turned on or off from the Simulation mode's and Commissioning mode's control bars.

OK

Saves and closes the dialog box.

Cancel

Closes the dialog box without applying the changes.

Opens the Help system.