Debugging - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Debugging functionality in simulation allows you to validate your logic.

When you start a simulation session, the Simulation Control Bar appears. The Control Bar is a convenient way to to control and view details about break conditions. Click View Break Conditions in the control bar to define break conditions, update break conditions, and delete break conditions.