Importing System Selection Preferences - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
About this task

To import System Selection preferences:

Procedure

  1. In the Preferences - System Selection screen, select the System Selection tree that matches the type you want to import.
  2. Click Import. The Open dialog box appears.
  3. Select the desired file to import.
    Note: You may need to browse to the location where you saved the file if you saved it to a different location from the default, or received the file from others.
  4. Click Open. The preferences file opens and populates the System Selection preferences tree.