Copying and Pasting Naming and Signal Preferences - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Procedure

  1. In the desired column, select the non-shaded cell you want to copy.
  2. Press Ctrl+C to copy the preference.
  3. Select the non-shaded cell to which you want to paste. To paste to multiple cells, click and drag multiple cells in the column.
  4. Press Ctrl+V to paste the preference.
    Notes:
    • To mass edit names, first filter on the gray-shaded columns for Application or Function.
    • Because the Signal column has a drop-down menu, you cannot use your mouse to select cells. Use the Shift and arrow keys on your keyboard to select the desired cells in this column to copy and paste.

      You also can move the Signal column to another location in the table after changing one of the items to the desired signal, and then use your mouse to select the cells to copy and paste.