See Setting Default Naming and Signal Preferences.
|
Field |
Description |
|---|---|
|
Filter Text Box |
Use to filter the content of the table. Type one or more letters appearing in the data you want to view. For example, to view heating preferences, type heat in the field. See the Filtering Naming and Signal Preferences section. |
|
Column Headers (Sorting) |
You can sort the contents in ascending/descending order. See the Sorting Naming and Signal Preferences section. |
|
Application Name Column |
Name of the application in which the object belongs. You cannot edit items in this column. |
|
Function Name Column |
Function of the object (for example, used for an Analog Input or for a command). You cannot edit items in this column. |
|
Derived Name Column |
Format of the object’s name. You cannot edit items in this column. An object name consists of a defined Object Name Prefix and a defined Object Name Suffix. The object name is created by combining them. For example, the Object Name Prefix BLDG added to the Object Name Suffix of SP results in an object name of BLDG-SP. |
|
Name Prefix Column |
Full prefix of the object name. You can edit items in this column. |
|
Name Suffix Column |
Full suffix of the object name. You can edit items in this column. |
|
Description Prefix Column |
Full prefix of the object’s Expanded ID. You can edit items in this column. |
|
Description Suffix Column |
Full suffix of the object’s Expanded ID. You can edit items in this column. |
|
Signal |
Default signal used for the application. See the Object Naming and Signal Preferences section. |
|
Reset |
Resets the selected row to the Johnson Controls standard default value. See the Resetting Naming and Signal Preferences section. |
|
Reset All |
Resets all rows to the Johnson Controls standard default values. See the Resetting Naming and Signal Preferences section. |
|
Import |
Opens a saved object naming preference file and populates the naming and signal preferences screen with its data. See the Import and Export Preferences section. |
|
Export |
Saves naming and signal preferences to a file so you can access it from the same computer for later use or you can copy the file to use on another computer. See theImport and Export Preferences section. |
|
Save |
Applies the changes and closes the Preferences - Naming and Signal screen. |
|
Close |
Closes the Preferences - Naming and Signal screen without applying the changes. |
|
|
Opens the Help system. |