Unit Preferences - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

You can set the units of measurement to use when working in the tool from the New System dialog box (File > New) during the System Selection process. After setting the units and closing the tool, the tool remembers the last unit’s setting. The selected units are used until you change them in the New System dialog box. See Selecting a System (Creating a New System) in the Configuring a System section.