Module Use in Applications (Status AND) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by this module:

Table 1. Status AND Uses in Application System Selection Trees
Module Instance Name Application
Pump Status AND Custom and Monitoring Supervisory Control Only Applications

To see a module's connections and how modules interact with it, view the Connections table.