Reliability (Sideloop Minimum Selector) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
Table 1. Sideloop Minimum Selector Reliability

Input

Behavior When Input Is Not Reliable

Input 1

The last Reliable value is used in the minimum selection.

Input 2

The last Reliable value is used in the minimum selection.