Sideloop Average Inputs - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This module averages the inputs to produce the output. The module accepts two inputs and outputs the average of the inputs. The user can add more inputs to the module.

You can view and modify the modules in this group’s logic.

To see this module’s connections and how modules interact with it: