Reliability (ZN-T Setpoint Determination) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
Table 1. ZN-T Setpoint Determination Reliability

Input

Behavior When Input Is Not Reliable

Hardware Setpoint

The Hardware Setpoint uses the last reliable value.

Hardware Setpoint Offset

The Hardware Setpoint Offset uses the last reliable value.

Network Setpoint

If the Remote Setpoint mode is Network Only, use the last reliable value.If the Remote Setpoint mode is Network with Hardware Backup, use the Hardware Setpoint.