Table 1 describes the attributes used by the VAV Dual Duct Variable Flow Endpoint Calculation modules.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
CD Min Flow |
Specifies the minimum flow for the cold duct. |
0 l/s, 0 cfm |
|
|
CD OA Percent |
Percent of the cold duct air that is outdoor air. |
20.0% |
|
|
Cooling Max Flow |
Contains the constant flow for the dual duct box. |
500 l/s, 1000 cfm |
|
|
EFFCD-MAXFLOW (Eff CD Max Flow) |
V |
Contains the required cold duct maximum flow. |
Display Units: l/s, cfm |
|
EFFCD-MINFLOW (Eff CD Min Flow) |
G, V |
Contains the required cold duct minimum flow. |
Display Units: l/s, cfm |
|
EFFHD-MAXFLOW (Eff HD Max Flow) |
V |
Contains the required hot duct maximum flow. |
Display Units: l/s, cfm |
|
EFFHD-MINFLOW (Eff HD Min Flow) |
V |
Contains the required hot duct minimum flow. |
Display Units: l/s, cfm |
|
HD Min Flow |
Specifies the minimum flow for the hot duct. |
0 l/s, 0 cfm |
|
|
HD OA Percent |
Percent of the hot duct air that is outdoor air. |
20.0% |
|
|
Heating Max Flow |
Specifies the constant flow for the dual duct box. |
500 l/s, 1000 cfm |
|
|
Min Flow Reset Type |
Defines the type of min flow reset strategy. When None is selected, the min flow values are the values at the appropriate inputs. When CO2 is selected, a proportional reset based on a CO2 setpoint and a CO2 proportional band determines the required min flow values. In both cases, the Occupancy Level and Ventilation Requirement can increase the minimum flows. |
None Set Name: None/CO2 |
|
|
MINFLOWCO2-PB (Proportional Band) |
Specifies the band that the CO2 level must increase above the Setpoint to produce the largest minimum flow values when the Min Flow Reset Type is other than None. |
400 ppm |
|
|
MINFLOWCO2-SP (Setpoint) |
Specifies the CO2 level that the process variable must exceed to begin resetting the minimum flows when the Min Flow Reset Type is other than None. |
700 ppm |
|
|
OCC-LEVEL (Occupancy Level) |
Number of people in the zone. |
0 |
|
|
Process Variable |
Contains the measured variable used to reset the minimum airflow when the Min Flow Reset Type is other than None. |
0 ppm |
|
|
Ventilation Requirement |
Outdoor airflow required per person (Occupancy Level). |
10 l/s, 20 cfm |