Discharge Air Setpoint Reset - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This module is designed to reset the discharge air temperature setpoint based on a reset process variable (typically the outdoor air temperature). The module has two inputs that define the temperature reset band (OA Reset A and OA Reset B), and two inputs that specify the DA-T setpoints at each end of that band (Discharge Air Low Limit and Discharge Air High Limit). This module has an output for the DAT-SP (Discharge Air Temperature Setpoint).

You can view and modify the modules in this group’s logic.