Attributes (Damper Minimum Position Determination) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Table 1 describes the attributes used by the Damper Minimum Position Determination modules.

Table 1. Damper Minimum Position Determination Attributes

Name

Type 1

Description

Default Value

Occupancy

 

Current Occupancy status of the unit.

Occupied

Set Name: Occ Effective

Occ Minimum OA Percent

 

Contains the desired damper minimum position during occupied or bypass mode.

10.0%

Minimum OA Position

G, V

Minimum damper position.

0.0%

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)