Degrees to Direction - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Degrees to Direction module converts analog degrees to compass point values (North, NorthNorthEast, and so on). This module accepts the wind direction inputs defined in the attributes section. The module outputs the current direction of the wind to an enumeration value using the Wind Direction 16 enumeration set. The Degrees to Direction module is implemented as a standard Control Activity.

Figure 1. Degrees to Direction

You can view and modify the modules in this group’s logic.