Attributes (Minimum Flow Calculation) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The following table describes the attributes used by the Minimum Flow Calculation modules.

Table 1. Minimum Flow Calculation Attributes

Name

Type 1

Description

Default Value

Min Flow

 

Indicates the lowest value sent to the output of the module.

0.0

Device X Command

 

Indicates the current command being sent to the controlled device (where X is 1-8).

Off

Set Name: Off/On

Device X Min Flow

 

Indicates the minimum flow required for the controlled device (where X is 1-8).

0.0

Output

G, V

Indicates the minimum flow value required for all devices that are currently On.

0.0

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)