Attributes (Flow Differential Calculation) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Table 1 describes the attributes used by the Flow Differential Calculation module.

Table 1. Flow Differential Calculation Attributes

Name

Type 1

Description

Default Value

CD-F, HD-F, or FLOW (Calculated Flow)

G, V

Contains the result of the subtraction with reliability.

Display Units: l/s, cfm

Contributing Flow

 

Measured flow to be subtracted from the Total Flow.

0 l/s, 0 cfm

Total Flow

 

Measured total flow.

0 l/s, 0 cfm

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)