Attributes (Status Alarm Determination) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Table 1 describes the attributes used by the Status Alarm Determination module.

Table 1. Status Alarm Determination Attributes

Name

Description

Default Value

Alarm

Indicates the current alarm status of the device.

Normal

Set Name: Normal/Alarm

Command

Indicates the current command to the device.

Off

Set Name: Off/On

Delay

Delay (time period) allowed to elapse after the device starts and before it indicates a fault.

30 seconds

Flow Status

Indicates the current status of the device. If Failsoft is True, the switch is set to Off when the input is not Reliable.

Off

Set Name: Off/On

Status

Indicates the current effective status of the device. When True, the device is commanded on and the Flow Status is on. This value is False when the Flow Status input is off.

False

See Primary States (Status Alarm Determination).