The following table describes the attributes used by the Dual Fan Status Alarm Determination modules.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Alarm - AND |
Current alarm status of both devices as a result of an AND function. |
Normal Set Name: Normal/Alarm |
|
|
Alarm - OR |
Current Alarm status of either device as a result of an OR function. |
Normal Set Name: Normal/Alarm |
|
|
Alarm 1 |
Current alarm status of the first device. |
Normal Set Name: Normal/Alarm |
|
|
Alarm 2 |
Current alarm status of the second device. |
Normal Set Name: Normal/Alarm |
|
|
Command |
The current command to the first device. |
Off Set Name: Off/On |
|
|
Command 2 |
The current command to the second device. |
Off Set Name: Off/On |
|
|
Delay |
Delay allowed for the device to start before indicating a fault. |
30 Seconds Display Precision: 1s |
|
|
Flow Status |
Current status of the first device.
Note: When you set Failsoft = True, the value for the switch automatically sets to OFF when the input is not Reliable.
|
Off Set Name: Off/On |
|
|
Flow Status2 |
Current status of the second device.
Note: When you set Failsoft = True, the value for the switch automatically sets to OFF when the input is not Reliable.
|
Off Set Name: Off/On |
|
|
Status - AND |
Current effective status of both devices as a result of an AND function. A true indicates that the device is commanded on and the Flow Status is on. The value is false when the Flow Status input is off. |
False |
|
|
Status - OR |
G |
Current Alarm status of either device as a result of an OR function. A True indicates that the device is commanded on and the Flow Status is on. The value is False when the Flow Status input is off. |
False |
|
Status 1 |
Current effective status of the first device. A True indicates that the device is commanded on and the Flow Status is on. The value is False when the Flow Status input is off. |
False |
|
|
Status 2 |
Current effective status of the second device. A True indicates that the device is commanded on and the Flow Status is on. The value is False when the Flow Status input is off. |
False |