The following table describes the attributes used by the Dual Fan Command OR modules.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Command |
This input represents the command being sent to the first device. |
Off Set Name: Off/On |
|
|
Command 2 |
This input represents the command being sent to the second device. |
Off Set Name: Off/On |
|
|
Output |
G |
This is the result of the OR operation. |
Off Set Name: Off/On |
1 B - BACnet Exposed Parameter, C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)