Module Use in Application (Analog Status Determination) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The application System Selection trees use the individual modules in this group with the names in the following table.

Table 1. Analog Status Determination Uses in Application System Selection Trees

Module Instance Name

Applications

Supply Fan Analog Status Determination

AHU 100% Outdoor Air Single Duct Applications

AHU Mixed Air Single Duct Applications

Exhaust Fan Analog Status Determination

AHU 100% Outdoor Air Single Duct Applications

Return Fan Analog Status Determination

AHU Mixed Air Single Duct Applications

Relief Fan Analog Status Determination

AHU Mixed Air Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.