Device Enable - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Device Enable group provides the ability to enable devices based on network commands or outdoor air temperature.

These modules are included in the Miscellaneous category because they typically, but not always, provide information to other State Generation modules rather than connecting directly to State Selection. Also, see the Device Enable category of modules in the State Generation Modules (State Generators) section.