The following table describes the attributes used by the Subtract modules:
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
CHWTEMP-DIFF or CHWFLOW-DIFF [Output (Float)] |
V |
Indicates the differential of Input 2 subtracted from Input 1. |
0 |
|
Input 1 |
Indicates the floating variable from which Input 2 is subtracted. |
0 |
|
|
Input 2 |
Indicates the variable that is subtracted from Input 1. |
0 |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)