Status OR - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Status OR module examines up to eight Enum inputs and one Boolean input, and outputs a unified Enum status for the input group, a Boolean output indicating whether any status equals ON, and a Boolean output indicating whether all statuses equal ON. The module accepts eight ON/OFF inputs and a cascaded input for cases where you need more than eight inputs, and has outputs for any input ON, all inputs ON, and status.

This module is implemented as a Control Activity.

You can view and modify the modules in this group’s logic.

Figure 1. Status OR Logic