The following table describes the attributes used by the Load Calculator modules:
|
Name |
Description |
Default Value |
|---|---|---|
|
Flow |
Volumetric flow rate of the media through the device. |
0 l/s, gpm Precision: 10ths Minimum value 0.0. If Flow is less than zero, the module should use zero for the calculations. |
|
Glycol Concentration |
If Media Type is Water-Ethylene Glycol or Water-Propylene Glycol, this indicates the percent (in weight) of the glycol component in the mixture. |
10.0% Precision: 10ths Minimum Value 10. Maximum Value 90.0 |
|
Heat Cool Mode |
Switch to change the sign of Load, such that a positive value of a Heating Load means energy added to the fluid and a positive value of a Cooling Load means energy removed from the media. Changing this causes the module to execute. |
Cooling Set Name: Heating/Cooling |
|
Load |
The calculated amount of energy added or removed from the fluid. |
0 kW, MBtu/h if Heat Cool Mode = Heating kW, Tons of Refrigeration if Heat Cool Mode is Cooling Precision: 10ths |
|
Media Type |
The type of fluid used in the system. Changing this causes the module to execute. |
Water Set Name: Load Media |
|
Temperature In |
Temperature of the fluid entering the device. |
0 °C, 0 °F Precision: 10ths |
|
Temperature Out |
Temperature of the fluid leaving the device. |
0 °C, °F Precision: 10ths |
|
Unit Set |
System of units. Changing this causes the module to execute. |
I Set Name: Unit; SET |