Attributes (Device Alarm) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by the Device Alarm modules:

Table 1. Device Alarm Attributes

Name

Type 1

Description

Default Value

Input n

 

Indicates the inputs to this module (where n is 1-8).

Normal

Set Name: Normal/Alarm

Maintenance Switch

G

Provides the result of the OR operation and any latching, as translated into the Disable/Enable value of the Maintenance Switch.

Enable

Set Name: Disable/Enable

Output

 

Provides the result of the OR operation and any latching.

Normal

Set Name: Normal/Alarm

Reset n

 

Indicates the inputs used to set the Output back to normal when Setup n is Manual (where n is 1-8).

Off

Set Name: Off/Reset

Setup n

 

Indicates the latching action for the specific input (where n is 1-8). When Setup n is Automatic, the Output is Alarm if the associated input is Alarm. If all inputs and Cascaded OR Input are Normal, the Output is Normal. When Setup is Manual, the Output is Alarm if the associated input is Alarm. If all inputs and Cascaded OR Input are Normal and Reset is set to Reset, the Output is set to Normal.

Automatic

Set Name: Reset Type

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)