Chiller Forced Upstage - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Chiller Forced Upstage module derates the current running chillers by comparing the CHW supply temp and flow to a setpoint. This module provides two Boolean outputs. One output sets the derate flag true or false based on its inputs. The other output issues a 5-second derate reset pulse 5 minutes after the derate flag transitions from true to false. This module is implemented as a control activity.

Figure 1. Chiller Forced Upstage