Attributes (CW Temperature Diff Calc) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The following table describes the attributes used by the CW Temperature Diff Calc modules:

Table 1. CW Temperature Diff Calc Attributes

Name

Type 1

Description

Default Value

ChlrX CW Entering Temp (Where X Is 1-8)

 

Indicates the entering condenser water temperature for the associated chiller.

0 °C, 0 °F

ChlrX CW Leaving Temp (Where X Is 1-8)

 

Indicates the leaving condenser water temperature for the associated chiller.

0 °C, 0 °F

Command X (Where X Is 1-8)

 

Indicates the current command of the associated chiller or pump.

Off

Set Name: Off/On

Output

G

Provides the result of the module’s calculation, which is the largest CW differential value output.

0.0

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)