Module Use in Applications (CHW Pump Differential Pressure Setpoint Reset) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. CHW Pump Differential Pressure Setpoint Reset Uses in Application System Selection Trees

Module Instance Name

Applications

CHW Pump Differential Pressure Setpoint Reset

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.