Module Use in Applications (Alarm OR) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use individual modules in this group using the names in the following table.

Table 1. Alarm OR Uses in Application System Selection Trees

Module Instance Name

Applications

Fire Damper Alarm OR

All Air Handling Unit Applications

To see a module's connections and how modules interact with it, view the Connections table.