Configuring a Tab Container - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
Controller Tool Help
- Product
- Controls > Control Tools > Controller Configuration Tool
- Document number
- LIT-12011147
- Version
- 13.1
- Revision date
- 2019-12-04
Procedure
-
In the Perspective Management dialog box, select the Tab container you want to configure.
-
Enter a Name and Description (optional) for the Tab container. The name appears in the UI, and the description appears as a tooltip when you hover over the component in the UI.
-
Select the Visible check box to show the container within the UI, or clear the check box to hide the container in the UI.
-
Click the Position drop-down list box to choose the location in the container for where the tabs appear. (See Figure 1 in Tab for examples.)
-
If the Tab container has subcomponents in the Display Order field, select the subcomponent and click the up arrow (
) or down arrow (
) to reorder the items.
-
Click Apply.
-
Click Close.