Configuring a Tab Container - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Procedure

  1. In the Perspective Management dialog box, select the Tab container you want to configure.
  2. Enter a Name and Description (optional) for the Tab container. The name appears in the UI, and the description appears as a tooltip when you hover over the component in the UI.
  3. Select the Visible check box to show the container within the UI, or clear the check box to hide the container in the UI.
  4. Click the Position drop-down list box to choose the location in the container for where the tabs appear. (See Figure 1 in Tab for examples.)
  5. If the Tab container has subcomponents in the Display Order field, select the subcomponent and click the up arrow () or down arrow () to reorder the items.
  6. Click Apply.
  7. Click Close.