The following table provides information on selections found in the table data custom configuration panel.
| Field | Description |
|---|---|
| Name |
Indicates the name that appears within the perspective UI. |
| Description |
Indicates the text included in the tooltip that appears within the UI when you hover over the widget's header. |
| Data Criteria Type |
UI Column: Enables you to select table data from a set of UI Column types. BACoid: Enables you to specify table data by BACoid. |
| Visible | Indicates if the widget appears within the UI. |
| Order |
Alphabetical: Specifies that table data appears in alphabetical order. As Defined: Specifies that table data appears in the order you defined the data. This order type applies more to the BACoid data criteria type. Note: When you specify that State Generator table data (UI Column) appear As Defined, the State Generator table data appears in the same order as the State Table.
|
| Settings - Show All | When selected, shows all points within the application. When cleared, shows only BACnet Exposed points.
Note: This attribute appears only when you have an application open.
|
| Expansion Level | Indicates the level of details that appear within the tree (1 to 5).
Note: This attribute appears only when you have an application open.
|
| Filter | Provides a text box to search the selection tree based on the node name. The search results include the matching node and its ancestors. |
|
|
Moves a subcomponent up in the display order. Applies when the Order property is set to As Defined.
Note: This attribute appears only when you have an application open.
|
|
|
Moves a subcomponent down in the display order. Applies when the Order property is set to As Defined.
Note: This attribute appears only when you have an application open.
|
| Object Identifier | Allows the user to manually define a BACoid to display in the widget. |
|
|
Adds the manually defined Object Identifier to the widget's list of BACoids. |
|
|
Removes the manually defined Object Identifier to the widget's list of BACoids. |
|
|
Removes the selected points in the list from the widget. |
|
|
Adds the selected points in the list to the widget. |