System Selection Information - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The System Selection Information widget provides a read-only view of your system design. This view enables you to see the system selection summary without the need for you to print a System Selection Summary report. The System Selection Information widget type does not support any data criteria types or any properties. For information on the System Selection wizard, see the System Selection Wizard in the Configuring a System section.