Logic View - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Logic View widget functionality is identical to the previous release's Logic tab. This widget does not need to appear as a tab and can be located anywhere within the UI. For more information, see Logic Tab.