Details Data - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Details Data widget shows the details of a module or point. This view is identical to the Details dialog box that appears when you view details of an item within the Classic View (Figure 1). The Details Data widget supports a single BACoid as the data criteria type, and does not allow hardware points, advanced objects, or elements of a primitive to appear as the main reference of the view. See BACoid for more information.

Note: A Missing Data message appears in this widget when the specified BACoid does not exist in the open application.
Figure 1. Details Dialog Box (Left) and Details Data Widget in Perspective (Right)