The Connections table appears in the Connection tab of the Features Panel in all modes. This table can show the connections for one or more modules and the State Selection tables. The Connections table displays the source and destination module and port data with the associated input and output connection of the selected module. In this table, inputs appear yellow and outputs appear turquoise.
In the Control tab, you can select to view connections for one module, multiple modules in a module category, State Selector only, or you can click Show All to view all connections.
In the Logic tab, you can select a module in the Activities tree to view the connections for the selected module. You can also select a module in the BACnet Exposed tab to view and update the Connections table.
For Inputs and Outputs, the default value appears after the input/output name during Configuration mode (for example, Present Value - False or Input - False). During Simulation and Commissioning mode, the current value/present value appears after the input/output name. The following table describes the right-click menu options of the Connections table.
|
Menu Option |
Context |
Description |
|---|---|---|
|
Break Connection |
Input Output |
Disconnects the current connection and leaves the connection blank. |
|
Change Connection |
Input Output |
Launches a dialog box allowing the user to choose from a tree of available blocks and ports. |
|
Expose Ports |
Selected Module Header |
Opens the Port Exposure dialog box to show or hide ports from connection. You cannot remove the selection for connected ports as such ports are disabled in this dialog box. |
|
Make Connection |
Input Output |
Launches a dialog box allowing the user to choose from a tree of available blocks and ports. |
|
Button or Check Box |
Description |
|---|---|
|
Show All |
Returns the Connections table to the default view, which is showing all module connections. |
| Show State Selector | When selected, this option shows only the State Selector. |
|
Expose Ports |
Opens the Port Exposure dialog box to hide ports from connection. You cannot remove the selection for connected ports as such ports are disabled in this dialog box. |
|
Freeze Connections |
Prevents the Connections table from dynamically changing as you select modules. |
See the Features Panel Screen section for a description of this table’s components.