System Configurations Tab - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The System Configurations tab allows you to manage your library of perspectives based upon all system configurations, or specific applications. See the following figure and table for a description of the System Configurations Tab.

Figure 1. System Configurations Tab

Table 1. System Configurations Tab
Field Description
System Configurations Tree Use to view all associated perspectives or system-based perspectives.
Associated Perspectives Pane Displays all associated perspectives and allows you to select or clear check boxes to configure associated perspectives.
Perspectives Provides a list of all associated perspectives for that system type. Perspectives are ordered alphabetically. You can click the column header to reverse the order of the list.
Apply Not used.
Close Closes the dialog box.
Opens the online help system.