Frame - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Frame container is only available at the perspective (or root level) and specifies that the subcomponents of information appear as frames. The name of each frame stems from the name of the associated perspective subcomponent. For example, the Classic View is a root frame container that defines the Application and the Features panels as frames.