CCT/PCT Commissioning Troubleshooting - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
To troubleshoot issues with CCT/PCT Commissioning, perform the following system checks:
  • Ensure that overrides are removed.
  • Ensure that output is not overridden in applications created at CCT/PCT Release 4.1 where no override monitoring feature is automatically created.
  • Ensure that output is not overridden in custom applications that lack added override monitoring.
  • View the details of the PID. Check the values of PRAC Proportional Band and PRAC Integral Time. If they are significantly different than the initial tuning parameters and the system is not controlling, reset PRAC+ Adaptive Tuning and monitor the system.