Systems Not Suited for PRAC+ - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
When PRAC+ is applied to certain systems for which it was not designed, the performance is less than ideal. PRAC+ was designed for the majority of linear first-order plus delay systems. While most mechanical systems that are encountered in the field match this description, for other systems, it may be desirable to turn off PRAC+ and manually tune the PID. Examples of these systems include: