Systems Controlled with a Sequencer - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The minimum on and off times of the sequencer create problems for PRAC+ adaptive tuning. Unless the minimum on and minimum off times are very short, the sequencer causes large cycling in the process variable. PRAC+ monitors these oscillations and tunes the PID controller to a sluggish state. It is not possible to configure the minimum tune band and the dead band of the PID to allow PRAC+ to tune these systems.