Systems Controlled with a Sequencer - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The minimum on and off times of the sequencer create problems for PRAC+ adaptive tuning. Unless the minimum on and minimum off times are very short, the sequencer causes large cycling in the process variable. PRAC+ monitors these oscillations and tunes the PID controller to a sluggish state. It is not possible to configure the minimum tune band and the dead band of the PID to allow PRAC+ to tune these systems.