The following table describes the attributes used by the Output Controller Last Value (Boolean, Enum, Float) modules:
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Input |
Contains a Default Value of this Input that is passed to the Present Value on the first execution after startup or enable. Otherwise, the Current Value of the Input is passed to the Present Value. |
False 1st Enum0.0 |
|
|
Present Value |
G, V |
Contains the output of this module |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)