Primary States (Sideloop Reset Output) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
  • Min: The Present Value is set to Output Range Low.

  • Max: The Present Value is set to Output Range High.

  • Control: The Input is spanned using the Input Range Low, Input Range High, Output Range Low, and Output Range High to produce the Present Value.