The following table describes the attributes used by the Sideloop Reset Output module.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Input |
Used to reset the desired setpoint for the process variable to be controlled to when commanded to Control. |
0.0 |
|
|
Mode |
Allows the state to be set to Min, Max, or Control. |
Control Set Name: Min/Max/Control |
|
|
Present Value |
V |
Contains the result of spanning the Input using the Input Range Low, Input Range High, Output Range Low, and Output Range High. |
|
|
SL-OUTA (Output Range Low) |
Used to set up the span when the mode is Control. This represents the Present Value when the Input is at or below the Input Range Low. |
0.0 |
|
|
SL-OUTB (Output Range High) |
Used to set up the span when the mode is Control. This represents the Output when the Input is at or above the Input Range High. |
0.0 |
|
|
SL-OUTSTATE (State) |
G, V |
Current State of the module. |
Set Name: Min/Max/Control |
|
SL-RSTA (Input Range Low) |
Used to set up the span when the mode is Control. This corresponds to the low x value. |
0.0 |
|
|
SL-RSTB (Input Range High) |
Used to set up the span when the mode is Control. This corresponds to the high x value. |
0.0 |